Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the various events in which M580 Hot Standby CPU causes switchover.
Any one of the following events will cause a switchover:
  • The primary PAC has encountered a blocking condition and entered the HALT state.
  • The primary PAC has detected an unrecoverable hardware or system error.
  • The primary PAC has received a STOP command from Control Expert or the DDDT.
  • An application program is being transferred to the primary CPU.
  • Primary PAC power is turned off; a power cycle occurs.
  • The following events simultaneously occur:
  • The primary PAC loses communication to all RIO drops.
  • The Hot Standby link is healthy.
  • The standby PAC maintains communication with at least one RIO drop.

Similar to a switchover, a swap is a controlled event that transfers control of the network from the primary PAC to the standby PAC. A swap can be caused by:
  • Execution of the DDDT CMD_SWAP command by either program logic, or an animation table Force command.
  • Manually clicking the HSBY Swap button in the Task tab of the CPU Animation window in Control Expert.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings