Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In MiCOM P14x Alarms Code Verify fail, Software failure are coming in event file.
Maintenance records are part of a self-diagnostic feature on MicomP40 relays. The relay internally does constant check on SRAM, EPROM, Program code, etc, if it detects any abnormality, the relay attempts to resolve it by performing a reboot and logs maintenance record in the event file.
The reboot is recorded as the power-on event which is as below
After re-boot, if the issue is not persisting, we treat this as healthy.
In the current case we observe we have one maintenance record & after reboot, the issue did not recur. The relays undergoing this phenomenon are perfectly healthy, not classified as defective.
As these are maintenance records, which denote the status as a healthy condition of the relay, and we would advise you to keep the relay in service.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings