Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to replace old cartridge in new base sepam series 80.
The Basic rule to find out whether a Sepam base module & memory cartridge module are compatible or not.
We need to check the major index of both base module & cartridge module, the major index of the base unit
the version must be greater than or equal to the major index of the cartridge-application version.

For Example, The base unit with a version V2.05 (major index = 2) and an application with a version V3.00 (major index = 3) are not compatible.
If this rule is not observed, a major fault occurs and Sepam displays the message
"Version not Compatible"

The SEPAM 80 base unit with base version greater than or equal to V8.01 and application version greater than or equal to V8.01 is compatible with the new Extended Memory Cartridge.
The Reference for the Extended Cartridge Memory is MMR120 59701.

Sepam series 60 and 80: As application type is in the cartridge, modification of the Sepam application type requires only replacement of the cartridge.
You need to order a new cartridge with the application type needed.
Note: be careful, since you may need to purchase additional CCA63x CT adapters, depending on which Application Types are involved.

Schneider Electric India

Attachment(s)
63230-216-247_MMS020_InstallSheet.pdf [391.57 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings