Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the diagnostic features available in M580 safety IOs.
Each M580 safety I/O module presents the following diagnostic features:-

1.Self-test at module start-up
2. Continuous built-in runtime self-test
3. Module and channel diagnostic LEDs
In addition, the digital safety I/O modules also perform wiring diagnostics.

Power On Self Test
At power up, the I/O modules perform an extended series of power on self-tests. If the result of
these tests are:
1. Successful: The modules are considered to be healthy and are operational.
2. Unsuccessful: The modules are not considered to be healthy and are not operational. In this
case, the inputs are set to 0, and the outputs are de-energized.

NOTE: If the 24 Vdc external power supply is not connected to a digital input or digital output module, the power on self-tests are not performed and the module does not start.

Continuous Built-In Tests
During runtime, the I/O modules continuously perform self-tests. The input modules verify that they
are able to read data from the sensors over the complete range. The output modules verify that the
actual state of the output is the same as the commanded state.

LEDs
Each safety I/O module provides module and channel LED diagnostics on the front face of the
module:
1. The top four LEDs (Run, Err, I/O, and Lck) together describe the state of the module.
2. The bottom two or four (depending on the module) rows of LEDs combine with the top four LEDs
to describe the state and health of each input or output channel.
Refer to the LED diagnostics topic for the following safety I/O modules for more information on the
how to read the LEDs for that module:
1. BMXSAI0410 safety analog input module.
2. BMXSDI1602 safety digital input module.
3. BMXSDO0802 safety digital output module .
4. BMXSRA0405 safety digital relay output module.

Wiring Diagnostics for Digital Modules
Both the safety digital input module and the safety digital output module can detect the following
channel wiring diagnostic conditions:
1. Open (or cut) wire.
2. Short circuit to the 0 V ground.
3. Short circuit to the 24 Vdc.
4. Crossed circuits between two channels.

NOTE: The availability of these diagnostic functions depends on the specific wiring design of the module to its field devices. Refer to the application wiring examples for the following safety digital
I/O modules for more information:
1. BMXSDI1602 safety digital input module.
2. BMXSDO0802 safety digital output module.

For more Refer the attachment.

Schneider Electric India

Attachment(s)
Diagnostics Overview for M580 Safety IO Modules.pdf [130.14 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings