Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many 140CRA31908 can be configured in a M580 system.
Up to 2x 140CRA31908 can be configured in a M580 system (managing 1 single S908 Bus)
  • Each 140CRA31908 must have a 140CRP93•00 configured
  • If the S908 master is not needed, then simply use the 140CRA31200 to create a Quantum EIO drop

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings