Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use BMENUA0100 OPC UA communication module in M580 Hot Standby configuration
Yes, in a Hot Standby configuration, a BMENUA0100 module is installed in each Hot Standby main local rack. Each BMENUA0100 module is configured with a unique, static IP address. The two BMENUA0100 modules will retain their IP addresses, and will not exchange IP addresses on a Hot Standby switchover or swap.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings