Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the pin assignment of RJ45 Serial Port of MC80 PLC?
The below lists the pin assignment of RJ45 connector:


RJ45 Pin No.    RS232 Signal Name              RS485 Signal Name
1                            RXD                                      Reserved
2                            TXD                                      Reserved
3                            RTS                                       Reserved
4                          Reserved                                         D1
5                          Reserved                                         D0
6                            CTS                                       Reserved
7                          5 V output                               5 V output
8                            GND                                        GND

NOTE: The RS232 4-wire, RS485 2-wire, and power supply cables all use the same RJ45 connectors. MC80 PLC can use TWDXCAISO module as an isolation solution.
􀁺 10.10: is a fixed value
􀁺 x: The last two fields in the default IP address are composed of the decimal equivalents of the last two hexadecimal bytes in the MAC address.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings