Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the pin assignment of RJ45 Ethernet port?
The following lists the pin assignment of the RJ45 Ethernet port:

Pin No.                        Signal Name
1                                     TD+
2                                     TD-
3                                     RD+
4                           Not connected
5                           Not connected
6                                     RD-
7                           Not connected
8                           Not connected

􀁺 10.10: is a fixed value
􀁺 x: The last two fields in the default IP address are composed of the decimal equivalents of the last two hexadecimal bytes in the MAC address.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings