Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the pin assignment of USB port of MC80 PLC?
The below table lists the pin assignment of USB port:

Pin No.                        Signal Name
1                                    VBUS
2                                       DM
3                                       DP
4                                   Reserved
5                                   Ground


NOTE: To avoid unexpected behavior of the PLC, always use one of the following shielded cable USB that
comply the international standard:
􀁺 BMX XCA USB 018
􀁺 BMX XCA USB 045
􀁺 10.10: is a fixed value
􀁺 x: The last two fields in the default IP address are composed of the decimal equivalents of the last two hexadecimal bytes in the MAC address.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings