Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible I can upgrade firmware of MC80 PLC using Serial port?
No, The Firmware upgrade cannot be performed with serial port connection􀁺 BMX XCA USB 018
􀁺 BMX XCA USB 045
􀁺 10.10: is a fixed value
􀁺 x: The last two fields in the default IP address are composed of the decimal equivalents of the last two hexadecimal bytes in the MAC address.

Schneider Electric India

Attachment(s)
MC80 System Bits.7z [281.96 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings