Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to perform autotune on the ATV320.

To perform motor auto-tuning on the drive, follow these steps:

🔧 Step-by-Step Instructions:

  1. Enter all motor parameters into the drive (such as rated current, voltage, frequency, etc.).
  2. Press the Menu button on the drive.
  3. Navigate to:
    CONF > FULL > DRC > ASY > TUN
  4. Set the tun parameter to Yes [Do tune].

⚙️ What Happens Next:

  • If the drive is in a suitable state, auto-tuning will begin immediately.
  • Once tuning is complete, the parameter will automatically change to No action (nO).
  • If the drive is not ready for tuning (e.g., due to its current state), the parameter will revert to No (nO), and you will need to repeat the operation.

📌 Important Note:

  • Ensure the drive is in a cool state before initiating the auto-tuning process for optimal results.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings