Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to perform autotune on the ATV930.
Autotuning is performed by parameter 'tun'. Set parameters in drive. After parameters are set,press menu button on drive and go to  [Complete settings]  > [Motor parameters] > [Motor data] > [Motor tune] > [TUN]
Select yes  [Do tune].
Auto-tuning is performed immediate if possible, then the parameter automatically changes to [No action] (nO). If the drive state does not allow the tune operation immediately, the parameter changes to [No] (nO) and the operation must be done again.

Note: For auto-tuning, drive should be in cool state.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings