Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we mount BMEXBP1002(H) ,BMXXBP1200(H) and BMEXBP1200(H) on a DIN rail.

No, BMEXBP1002(H) ,BMXXBP1200(H) and BMEXBP1200(H) backplane can not be mounted on Din rail as these backplanes do not have springs like the ones shown in the legend (item 2) in below picture. on a DIN rail.

Rack

Racks longer than 400 mm (15.75 in.) that support more than 8 module slots are not compatible with DIN rail mounting

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings