Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to check CPU load for M580 system in EcoStruxure Control Expert.

M580 CPU load can be check through below path by connecting CPU with EcoStruxure Control Expert v14.1:

Double click on CPU> Animation> Task Tab

This info is available only for M580 with SV >= 2.80: percentage of the CPU load used by the task.
And EcoStruxure Control Expert v 14.1 or higher.
In addition to these values the system and total CPU load are given below the tasks checking field.  Refer below Picture:

T1

Also CPU Load related to system and tasks can be get through System word %SW110 to %SW116. Details are as per below picture:

T2




Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings