Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
what is max fault that 200A sensor can take without saturation?

The CT saturation current level is not published by R&D. However, we guarantee that the VIP400 will operate as specified in the manual. For example, if you make a Phase Overcurrent setting at 2 times Nominal Current with IDMT curves, the trip time will be within specifications, even if CT saturation occurs.

As per the VIP400 manual, the Phase Current inputs can withstand a fault level of 25kA for 2 seconds at room temperature.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings