Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to troubleshoot Communication issue in ComX 510 and ComX210

FAQ Title: How to troubleshoot Communication issue in ComX 510 and ComX210

Category: Troubleshooting, Technical assistance, electrical distribution, substation, Gateway, Communication issue, ComX, Energy management solutions,

Available to: Internal

Issue: Gateway Is offline/ not communicating to EAA

Product line: ComX 510, ComX 210

Environment: EAA-ED, Remote monitoring

Cause:  If the Gate way is Offline / not communicating, there are mainly three reasons involved in this.

1.      Internet issue -Internet may not be running due to that, the COMX is not communicating to EAA.

2.      Power OFF- There may be a chance of turning OFF the switch which is powered to the COMX.

3.      COMX Hang, software & hardware changes.

Resolution:

1. Internet issue.

If an Ethernet connection is used for publication, check:

-       that the Ethernet LAN cables are not disconnected. if ethernet LED’s are not blinking

-       the IP settings in the Settings > General Settings > Network Settings page.

-       the proxy settings in the Settings > General Settings > Proxy Settings page. Confirm there is no proxy presently configured. If a proxy is configured, consult your network administrator.

If a GPRS connection is used for publication,

-       Validate GPRS Signal is at minimum 3/4 on the ComX Web page. If signal is below this level, increase signal via an external antenna by adjusting the antenna position accordingly.

-       Power down the Com'X 510. Reinsert the GPRS modem and power up the Com'X 510

-       Check that the settings such as the APN are correct.

-       Check that protocol settings are correct in General Setting > Publication.

If a Wi-Fi connection is used for publication,

-       Power down the Com'X 510. Reinsert again the Wi-Fi USB key and power up the Com'X 510 if Wi-Fi USB key is not detected and USB key LED is not flashing.

-       Check that the settings such as the SSID name and the WPA2 key are correct.

2. Power Off.

-       Check the input power supply to the ComX, Check LED status it should e green.

3. ComX Hang: Reboot required for following cases;

-       Upgrading the firmware.

-       Restoring a configuration.

-       Changing the Ethernet network settings between 2 switched ports and 2 separate ports.

-       Inserting a GPRS modem.

-       Installing a Zigbee key

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings