Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the execution priority of different tasks in Unity Pro
One can define maximum 1 Mast, 1 Fast, 4 Auxiliary (only for Quantum & Premium), and 128 Event tasks.
The Priority of execution is as below:

up
Note:
If one is using Auxiliary task, Mast task has to be periodic.
Event task can be triggered by the event timer or through an input signal from the HLI module. Within the Event tasks there is again a hierarchy of priorities.

up1

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings