Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What do if there is "HOT" error code on display for Easy UPS SRV5KRIL-IN
Probable cause:

Temperature of the unit is rising above the set limits.

Possible Solution:

1. Disconnect non-essential equipment from the Easy-UPS to reduce the Easy-UPS load.
2. Maintain operating temperature between 0° to 40°C at full load and 40° to 50°C linearly derated to 75% of load.
3. Do not operate UPS where there is excessive dust or where the temperature or humidity are outside specified limits.
4. Do manual restart of UPS by switching off the output, disconnecting battery cable at the rear panel, turning off the input power supply and reconnecting the battery cable and input, this should make fault to be cleared.

In case if error persist even after trying the above troubleshooting, log the complaint.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings