Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many batteries can be connected to SRCE6KUXI?
1. Connect sixteen(16) SMF or tubular/flooded 12 V batteries in series.
2. The UPS is intended for use with 192 VDC nominal battery voltage. The external battery system connected to the UPS must not exceed 192 VDC nominal voltage.
3. Multiple strings of each 192 VDC can be connected in parallel.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings