Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the performance and capability for functions in BMENOR2200H Step2.
Module performance and capability for functions in step2 are:

Maximum number of bytes for data IN flow variables: 8000
Maximum number of bytes for data OUT flow variables:  8000
Maximum Event sync between HSBY modules per second: 4000
Maximum IEC104 Server connections when RTU act as Client: 64
Maximum IEC104 Client connections when RTU act as Server: 4
Maximum Event Buffer size: 150,000 events
Maximum NOR modules per CPU: 4 (based on CPU level and other ETH module Qty.)

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings