How to create a button from an image in machine expert software?
In machine expert visualization, it is possible to create a button or switch from an external image. Follow the below steps to add your customized button in the project:
1. First add the image on the image pool.

2. Insert the button on the visualization page of your project.

3. Click on the image and check the properties tab on the right.


4. Go to Input Configuration-->OnMouseDown, and insert the variable that you want to toggle with the button. In this case 'lamp' is the variable that will change state on the click of button.
5. Check the operation on simulation mode or web visualization of the controller.

1. First add the image on the image pool.
2. Insert the button on the visualization page of your project.
3. Click on the image and check the properties tab on the right.
4. Go to Input Configuration-->OnMouseDown, and insert the variable that you want to toggle with the button. In this case 'lamp' is the variable that will change state on the click of button.
5. Check the operation on simulation mode or web visualization of the controller.
Released for: Schneider Electric India




Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.