Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does BMXERT1604.2 is compatible with CE 14.1 for M580 Hot Standby CPU.
BMXERT1604.2 with EcoStruxure Control Expert v14.1 is only supported with Standalone CPU with CRA version 2.1 or above and not supported with M580 HSBY.
However, it is supported with M580 Safety HSBY SV 3.10 and CRA V2.30 or higher.

For M580 HSBY, BMXERT1604.2 will be supported with EcoStruxure Control Expert v 15. There is no hotfix for Control Expert v14.1


Refer the attached Firmware history of BMXERT1604 for more details on compatibility.

Schneider Electric India

Attachment(s)
BMXERT1604T Firmware History_SV02.10 (1).pdf [79.36 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings