Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the Built-in protections available with BMXDDO6402K module.
Below are the various Built-in protection available with BMXDDO6402K IO module:

Against over voltage: Yes, by Transil diode

Against inversions:    Yes, by inverted diode ,Provide a 2 A fuse to the +24 V pre-actuator supply.

Against short-circuits and overloads : Yes, by current limiter and electric circuit-breaker 0.125 A < Id < 0.185 A

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings