How can we help you today?

Where can I found compatibility between Control Expert Versions, Application Versions and PLC OS for premium plc.

Overview

Application version corresponds to the processor OS version displayed in Control Expert configuration screen.
The OS version corresponds to the minimum version required to execute an application functional level.
Higher OS versions provide compatibility with a lower application version.
For example, a Quantum application version V2.00 generated by Unity Pro V3.0 can be executed by a PLC OS version V2.40.
NOTE: Unity Pro is the former name of Control Expert for version 13.1 or earlier.
Modicon Premium Platform

This table gives the application version created with the different Control Expert/Unity Pro versions:
Minimum OS versionUnity Pro / Control Expert
V2.0V2.1V2.2V2.3 SP1V3.0V3.1V4.0V4.1V5.0V6.0V6.1V7.0V8.0V8.1...V15.0
TSX H57 •4MNA2.502.702.903.003.10
TSX P57 ••4M2.002.302.602.903.003.10
TSX P57 0244M2.002.302.602.903.003.10
TSX P57 1634M2.002.302.602.903.003.10
TSX P57 2634M2.002.302.602.903.003.10
TSX P57 3634M2.002.302.602.903.003.10
TSX P57 4634M2.002.302.602.903.003.10
TSX P57 5634M2.002.212.302.602.903.003.10
TSX P57 6634MNA2.402.602.903.003.10
TSX P57C • 0244MNA2.302.602.903.003.10
TSX PCI57 ••4MNA2.302.602.903.003.10

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings