The diagram below shows a three-wire actuator with an optional wiring scheme for broken wire detection. The dotted line reads back whether or not current has reached the actuator. When the output on pin 6, row 2, is high, the input from pin 6, row 1, must also be high.
Separate connections to pins 17 and 18 are shown on row 3, even though these two pins are internally connected. This is done to halve the load.
Separate connections to pins 17 and 18 are shown on row 3, even though these two pins are internally connected. This is done to halve the load.
Released for: Schneider Electric India