What Is Tropicalization and tropicalization category T2 with respect to IEC 60068 standard?
The Tropicalization term is related to the damp heat environmental conditions.
It means the product have been internally testing based on damp heat cycling test according to IEC 60068-2-30 Std (Test Db) as per severity 2 : cyclic test at 55°C and 95% relative humidity, two 24h cycles (12h + 12h).”
Released for: Schneider Electric India