Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is AL517 error in Lexium28/26 drives

AL517 means Encoder overvoltage or overcurrent.

AL517 trigger condition: The current supplied by the drive for the 5 V encoder supply has exceeded the limit.

This condition may occur up to three times in succession. After the third time, a time delay of one second must pass before the power stage can be enabled again.

So , AL517 is hardware issue ( could be cable , drive ,motor)

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings