Video: How to program ATV logic in ATV320 drive using somove
This video demonstrates how to use and program ATV logic in ATV320 using somove.
1. Open ATV320 somove file.
2.Go to ATV logic tab on somove.
3. Program ATV logic program using function blocks and assigning inputs and outputs to drive parameters.
4. Save the somove file and download in the drive.