How can we help you today?

Can we install SmartX AS-P servers vertically in DDC panel.

Always install the terminal base on a horizontal DIN rail. This position is required to provide sufficient cooling air flow through the electronics module. Installation on a vertical DIN rail can significantly reduce the life span of the module.

Refer attached image.

Schneider Electric India

Attachment(s)
AS-P Mounting.png [165.58 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings