Video: How to change Max Frequency in ATV630 Drive
This Video shows how to change Max Frequency in ATV630 Drive as sometime user want to change the maximum frequency (HSP) of drive as per Motor plate description.
By default HSP :- 50 Hz
You want to modify this to 60 or more than 50 HZ.
In that case first you need to modify Max Speed (tfr) parameter then modify HSP <=tfr.
If you will not modify the max speed then you would be not able to change HSP (High speed) more than the max frequency (tfr) setting