Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to do the PTO configuration in M221/M200 PLC
This video demonstrates how to do the PTO configuration in M221/M200 PLC  , EcoStruxure Machine Expert basic is used for programming TM221 logic controller and Easy Line Controller.
This video helps you on how to generate pulse train output through M221/M200 PLC and used for different servo drives.

EcoStruxure Machine Expert Basic can be used for programming of TM221 , TM200 Logic controllers and TM100 controller. Pulse train output are used for basic motion application
where in the servo drive run with the help of pulse generated from PLC.


Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings