Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
UPS SRV3KUXI-IN is not working on Generator?
Probable causes:

1. Input Voltage or Frequency not in the range.
2. Input voltage Waveform type is not a pure sine wave.
3. Capacity of the generator is less than the UPS capacity.

Possible Solution:

1. Make sure Input Voltage is 230v and Frequency is 50hz.
2. Input waveform type should be a pure sine wave.
3. Capacity of the generator should be 1.5 times more than the UPS capacity.
In case if the issue persists even after trying the above troubleshooting, log the complaint.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings