Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What do if there is BDC error code on display for Easy UPS SRV3KUXI-IN ?
Probable cause:

The battery is loosely connected, the battery is not connected or the battery is weak.

Possible Solution:

1. Check whether the battery is connected to the UPS by removing the front bezel. If not connected snap the battery connectors together.
2. Allow the battery to charge for 5hours.
3. Execute the battery self-test by navigating through the SET option to confirm the battery status.
4. Error gets cleared if the battery passes the self-test. If the battery fails the self-test, then batteries need to be checked.

In case the error persists even after trying the above troubleshooting, log the complaint.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings