Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video - How to use file system download method in EOTE

You can transfer (PC to Panel) the project files to the panel through the external storage device.

1. Start the screen editing software on the PC and open the project that you want to transfer (PC to

Panel).

2. In Project Explorer window, go to [System Architecture] and click [Target01].

3. In Properties window, go to [Function] tab ➞ [Basic] tab and acknowledge that [Type] in [Transfer

Method] is [File System].

4. In [Project File], click icon with three dots and select the folder where the file Package.VML is saved.

5. On the Application toolbar, click with download icon.

6. The Download Manager dialog box displays the status. When the transfer is complete, the file package.VML is generated in the destination folder. If the destination folder is outside external storage, copy the file to the external storage folder.

7. Close the Download Manager dialog box after the transfer is complete.

8. Turn on the panel.

9. Insert the external storage in the panel.

10. Open Hardware Configuration screen and touch [USB]/[SD]/[Local Storage] in [Download from].

After the project has been transferred successfully, the panel restarts and runs the transferred project.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings