Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the general instructions and limitations of CCOTF for an M580 Safety PAC?
CCOTF ( Changing a Configuration on the Fly) for an M580 Safety

The change configuration on the fly (CCOTF) feature makes it possible to change a Control Expert configuration while the PAC is running. Supported functions can include:
• Adding a drop.
• Adding an I/O module.
• Deleting an I/O module.
• Editing the configuration of an I/O module, including:
◦ Change a parameter setting.
◦ Add a channel function.
◦ Delete a channel function.
◦ Change a channel function.

NOTE: CCOTF functions do not apply to CIP Safety devices.
The CCOTF feature is enabled by selecting Online modification in RUN or STOP in the Configuration tab of the CPU module.
The basic functionality of CCOTF has been implemented in the M580 safety PAC, with the limitations described below.


Limitations of CCOTF for an M580 Safety PAC

The CCOTF feature is implemented in the M580 safety PAC, with limitations that are based on the specific function and type of I/O module, as follows:

Limitation

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings