Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Magnify and Reduce the Workspace View, in ESx Topology Manager?

To magnify or reduce the workspace view gradually, use the following method.

Ctrl + Mouse wheel up

Zoom in.
The position of the pointer becomes the center of the magnification.
Maximum zoom level is 400%.

Ctrl + Mouse wheel down

Zoom out.
The position of the pointer becomes the center of the reduction.
Minimum zoom level is 10%.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings