How can we help you today?

What are the System requirement for EcoStruxure Machine Expert-HVAC.

EcoStruxure Machine Expert - HVAC can be installed on a personal computer having the following characteristics:

Operative System
• Windows 8 / 8.1 64 Bit
• Windows 10 64 Bit

Hardware requirements
• Processor      Intel Pentium 1.6 GHz processor or greater
• RAM              1 GB; 2 GB preferred
• Hard Disk      500 MB hard disk space for a default installation; allow a further 1 GB hard disk space for installing libraries and dedicated applications
• Peripherals    Mouse or compatible pointing device
• Peripherals    USB interface
• Web access   Web registration requires Internet access

EcoStruxure Machine Expert - HVAC requires Administrator rights to be installed.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings