Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the limitations/Restrictions of GP-Pro EX Global D-Script?

Restrictions Specific to global D-Script are below:

  • Global D-Script operation is suspended during screen changes or other GP operations.
  • After the display unit is turned ON, Global D-Script actions are not performed until all data reads are completed for the initial screen.
  • After the initial screen changes, Global D-Script actions may be performed before the data reads are completed.
  • The maximum number of devices in the Global D-Script is 255. (Total number of devices used in trigger expressions and script programs.)
  • D-Script with 256 or more devices do not run. Since these devices always read data regardless of the screens, be sure to use only the minimum number of devices required by your D-Script. Otherwise, operation performance can be degraded.
  • The maximum number of Global D-Scripts is 32. The currently used function also counts as one Global D-Script. When the number of Global D-Scripts reaches 32, any subsequent Global D-Scripts are ignored.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings