How can we help you today?

What are different DHCP Server Options available with BACnet/IP controllers.

The following DHCP server options are supported with BACnet/IP controllers:

- AS-P server or AS-B server with DHCP on a private IP network

- Router or switch with DHCP on a private IP network

- Computer with DHCP on a site IP network

NOTE:

These options are topology independent. A router or switch or a computer on a local network are similar since both involve a local network connection. Be sure to locate only one of these configurations on a network segment at the same time, however. From a network management view, it is not desirable to have more than 1 DHCP server assigning addresses and responding to requests.

Please refer below EBO webhelp link to see above options in more details;

https://ecostruxure-building-help.se.com/bms/topics/show.castle?id=12105&locale=en-US&productversion=2022&a=1

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings