Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the tasks which can be performed for BACnet/IP controllers using Commission mobile application.

You can use the Commission mobile application to perform below tasks:

- Configure IP and BACnet device settings

- Change the Ethernet switch mode

- Configure the system time (in standalone mode)

- Store and upload device common settings

- View status information

- Generate diagnostic reports

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings