How can we help you today?

What is Initial IP address assignment process workflow for BACnet/IP controllers.

When the BACnet/IP controller is powered up, it undergoes a process to determine the IP address settings it needs for IP communication. This helps minimize the time required for the module to fully boot to normal operation.

NOTE: For convenience during engineering and initial commissioning, you can directly connect the BACnet/IP controller to a laptop computer.

Please refer below illustration for IP address assignment workflow;

IP assignment workflow

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings