Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to reassign IP address in case BACnet/IP controller detects an IP conflict while assigned a static IP address.

You can reassign IP address by using any of the following methods:

- Temporarily reconfigure the IP network of the host server to an IP in the Auto-IP range to discover and correct the IP address

- Connect an additional Enterprise server to the network with a BACnet IP network configured in the Auto-IP range to discover and correct the controller's IP address

- Connect the Commission mobile application to the network using an IP address configured in the Auto-IP range to discover and correct the controller's IP address

- Connect the Commission mobile application to the BACnet/IP controller using the Bluetooth Adapter on any SpaceLogic Sensor connected directly to the controller to discover and correct the controller's IP address

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings