How can we help you today?

How EcoStruxure Building Operation Servers communicate with each other and the WorkStation.

EcoStruxure BMS servers can use three different communication protocols:

TCP is fast and you can set up domain authentication which makes for easy, yet secure access.

HTTP is slower than TCP but better for accessing resources outside the LAN/firewalls.

HTTPS is slower than HTTP but safer for accessing resources outside the LAN/firewalls.

Each EcoStruxure BMS servers listens on three communication ports, one for each communication protocol:

TCP on port 4444 (fixed)

HTTP on port 80 (default)

HTTPS on port 443 (default)

WorkStation Communication to EcoStruxure BMS servers);

HTTP - Non-binary, port configurable, default 80

HTTPS - Encrypted supporting TLS 1.2, port configurable (default 443)

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings