How can we help you today?

How to import logic and configuration project from Geo SCADA / SCADAPack x70 configuration export?

To import logic and configuration project from Geo Scada / SCADAPack x70 configuration export, refer below steps.
  1. Under My Network, right-click on SCADAPack x70 Controller Settings -DeviceDTM and select Additional Functions > Import Logic Project.
  2. In the Import Logic Project dialog, click Browse to navigate to the file. An archived logic project file has one of the extensions .XEF, .ZEF, or .STA. Exported task logic content has a .xpg extension.
  3. In the Open dialog, locate the file that you want to import, then click Open.
  4. In the Import Logic Project dialog, click Ok. A confirmation dialog is displayed when the operation successfully completes.
  5. Click Ok. If the .STA project is password protected, the Password dialog opens.
  6. Enter the password for the project and click Ok.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings