Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Getting message "External Power supply is required" in the power supply budget of BMXCPS3020 .
The M340 DC power supplies do not supply any 24 VDC for External field devices or BMXCPS2010 or 3020 power supply has no inbuilt sensor DC supply 24 VDC to be fed sensors.
The warning is to ensure customer that he need to supply external power supply to power the I/O.
It is a warning because you have this anyway need a separate 24VDC power supply in the system and the system gives a kind of advice. It is also displayed neatly, the bar is orange in color and is in the legend "External power supply required".

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings