Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Easy 3L Power Block logs are recording a temperature out-of-tolerance alarm or over temperature
Issue:
During normal operation with a load between 50 to 100% load and due to low fan speed or other causes, it is possible to get the temperature out of tolerance alarms
Environment:
Startup phase, FSR testing UPS with load, HVAC design and implementation, Break Fix, Temperature alarms activated in the UPS or UPS room. Normal operating status with loads. Loads from 40% to 100%, typically 50% to 75% if the fan speed is low.
Possible Cause:
  • The power block inverter heatsink temperature is out of tolerance
  • The power block PFC heatsink temperature is out of tolerance
  • The temperature sensor could be faulty inside the power block.
These alarms can be pre-activated for the following reasons or a combination of reasons:
  • The UPS has two ambient temperature sensors. The first is installed on the back of the front panel, and the second is installed on the bypass block control board as a backup.
  • If the temperature is over 35℃, the ambient temperature sensors monitor the ambient temperature and control the cooling fan's speed.
  • The placement of the HVAC system and back pressure affect the UPS fans' ability to pull air from the front.

Resolution:
  • Check for airflow restrictions in front of each power block.
  • Verify all fans are working and pushing air toward the Power Blocks.
  • As a contributing factor, check the room's ambient temperature and load percentage.
  • Verify the HVAC room's back pressure condition as the main contributor or as an additional contributor.
  • Check the UPS exhaust sections for restrictions and turbulent airflow.
Caution: If the ambient temperature in the UPS room crosses 40°C, the UPS load will shift to bypass operation.

Note: If the above conditions meet, then an FSR visit is required to check the UPS parameters and Event logs. Please contact Schneider Electric.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings