How can we help you today?

Why is XA2-EVF*LC references not working on 110VDC.

As per the supply voltage specification mentioned in datasheet and catalogue the new products of XA2-EVF*LC are designed to work with 110VAC/DC Supply.
This is due to the improvement made in the product of XA2-EVF*LC. The old product only can be used in 110V AC.

How do you identify an old product?
We need to check the data code of these product. It can be found like below attached.

The data code 8A21304 (means the date is year 2021 week 30) is the new product.
Kindly note that the data code before 8A20433 can't be used in 110V DC system.

Schneider Electric India

Attachment(s)
Lamp.jpg [182.83 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings