Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it normal to have visible flash, when Aux trip unit Acti9 iMX is energized?

Yes, when Aux trip unit Acti9 iMX is energized there is an inrush current due to coil circuit. So you could have an external visible flash (refer attached image) inside its internal circuitry during its operation but that's completely normal.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings