Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where we can change setting of "enable IP ping for SP-C controller" in security expert?

SP-C controller does not reply the ping request because ping is disabled by default for the Ethernet connection on SP-C.

Ping request can be re-enabled via Controller Command in Security expert application.

Solution:-

Below are the steps to re-enable the ping command thru security expert application:-

Open security expert application, Go to Site >> controller >> General >> Command

Image1

Expand the Commands tab and set command “EnablePing = true” as mentioned in below snap.

Image2

Note:- For security it should be disabled after by entering EnablePing=false in the controller's Commands window and Save.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings