Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is Energy Monitoring device (EMD)?

Energy monitoring device (ENMOD1P) is a 6 Channel 1 pole communication energy monitoring device. It is compatible to Acti9 and Easy9 bottom feed bi-connect MCB with busbar relief, or any other make of MCB rating up to 80 A. With its ability to wirelessly connect to Wi-Fi, it enables convenient circuit monitoring.

  • Commercial Reference: ENMOD1P
  • Supporting Environment: Android and iOS

The performance category is Class 2.
You can mount ENMOD1P on the DIN rail along with protection device in the distribution board.

The key features of ENMOD1P are:
It accurately measures real-time values of:

  • Voltage
  • Current
  • Power factor
  • Active power
  • Apparent power
  • Reactive power
  • Active energy
  • Apparent energy
  • Reactive energy

Through the Wiser application for iOS and Android, ENMOD1P provides:

  • Support for data availability.
  • Overall Energy Management
  • Load Monitoring

You can use these features to access and monitor the data for the connected circuits.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings